Part Number: LMX2491
Tool/software:
Hi team,
customer used LMX2491 as FMCW modulation with below register configuration. The scanning frequency is from 1.5Ghz to 1.515625GHz. The issue is CPout=0V, and TRIG1 is high. And this is a occasional issue. could you pls help to check the configuration and see if any problem here? Thanks!
| Register | Value |
| 92 | 0x74 |
| 91 | 0x00 |
| 90 | 0x00 |
| 89 | 0x00 |
| 88 | 0x00 |
| 87 | 0x00 |
| 86 | 0x00 |
| 99 | 0x40 |
| 98 | 0x17 |
| 97 | 0x70 |
| 96 | 0x3F |
| 95 | 0XFF |
| 94 | 0XEE |
| 93 | 0XF0 |
| 106 | 0X80 |
| 105 | 0X19 |
| 104 | 0X78 |
| 103 | 0X00 |
| 102 | 0X00 |
| 101 | 0X00 |
| 100 | 0X00 |
| 113 | 0X23 |
| 112 | 0X30 |
| 111 | 0XC0 |
| 110 | 0X00 |
| 109 | 0X00 |
| 108 | 0X08 |
| 107 | 0X34 |
| 120 | 0X64 |
| 119 | 0X00 |
| 118 | 0X01 |
| 117 | 0X00 |
| 116 | 0X00 |
| 115 | 0X00 |
| 114 | 0X00 |
| 24 | 0XFF |
| 23 | 0XFF |
| 22 | 0XFF |
| 21 | 0X80 |
| 20 | 0X00 |
| 19 | 0X00 |
| 18 | 0X2C |
| 17 | 0X00 |
| 16 | 0X25 |
| 84 | 0X20 |
| 83 | 0X05 |
| 82 | 0X02 |
| 81 | 0XD8 |
| 80 | 0X33 |
| 79 | 0X33 |
| 78 | 0X00 |
| 77 | 0X7F |
| 76 | 0XCC |
| 75 | 0XCC |
| 74 | 0XDA |
| 73 | 0X80 |
| 72 | 0X00 |
| 71 | 0X00 |
| 70 | 0X24 |
| 69 | 0X00 |
| 68 | 0X02 |
| 67 | 0XD8 |
| 66 | 0X00 |
| 65 | 0X00 |
| 64 | 0X00 |
| 63 | 0X00 |
| 62 | 0X80 |
| 61 | 0X00 |
| 60 | 0X00 |
| 59 | 0X02 |
| 58 | 0X01 |
| 39 | 0X3A |
| 38 | 0XFA |
| 37 | 0X17 |
| 36 | 0X5A |
| 35 | 0X41 |
| 34 | 0X84 |
| 33 | 0X20 |
| 32 | 0X00 |
| 31 | 0X2A |
| 30 | 0X06 |
| 29 | 0X00 |
| 28 | 0X14 |
| 27 | 0X08 |
| 26 | 0X00 |
| 25 | 0X01 |
| 2 | 0X02 |
Rayna