Tool/software:
Hi,
I have a few more questions re: LMK03318:
- How can I make the differential outputs from an output bank to be in phase when configured as LVCMOS? What register bit do I need to set?
- If I want to use a TCXO (clipped sinewave) as my input reference, which input channel, primary or secondary, is more suitable?
- Output_0_1 pair and Output_2_3 pair: Is it possible to set output 0 (or 1) as 1.8V LVCMOS and output 1 (or 0) as 3.3 LVPECL with VDDO_01 set at 3.3V? Or, is this not recommended at all? There is only 1 output divider shared between two outputs for these banks and hence, these are not independent.
Thanks.
Prasoon