Part Number: LMG2100R044
Tool/software:
Hello. My name is Steve, and I am designing with TI LMG2100R044.
Currently, I am operating GaN driver by inputting two different frequencies using LMG2100R044.
One is inputting 7.25MHz frequency and the other is inputting 2MHz frequency and operating GaN driver.
The circuit part that inputs 2MHz frequency and outputs GaN driver operates normally and can confirm the output,
But the circuit part that inputs 7.25MHz frequency and outputs GaN driver does not operate normally.
It operates as if it is shorted (consuming 3.5A momentarily), and there is no actual circuit short in the circuit or PCB.
It seems to be a dead time issue. If the dead time is increased significantly so that the 7.25 MHz signal does not enter the input of the GaN driver, even if a 35 V power supply is applied,
the IC does not experience overcurrent, but if the dead time is gradually reduced so that the 7.25 MHz signal enters the input, an overcurrent occurs that causes a short circuit.
The part that receives the 2 MHz frequency input can check the output because the GaN driver operates normally, but the part that receives the 7.25 MHz frequency input
I do not know why the GaN driver does not operate normally.
Please check.
Thank you.