This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: LMX2592 CHIP RELATED INFORMATION

Part Number: LMX2592
Other Parts Discussed in Thread: LMX2572

Tool/software:

Hi

a) we are using for 3 LMX2592 chips in our application

1. PLL1 used for 30.72 MHz and required only sine wave, is it possible?

2. PLL2 used for 1.6GHz to 3.6GHz and required sine wave form

3. PLL3 used for 20 MHz to 8GHz required sine wave form only

above 3 conditions we required all are possible or not?

b) please provide the Gerber file for LMX2592 & Required Layer Stack up for our reference.

Regards

P Prasanth