This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2615-SP: LMX2615-SP

Part Number: LMX2615-SP

Tool/software:

I want to generate 65.472 when the reference clock is 10.23 MHz.

I made the output clock using the TICS Pro.

However, it does not work.

I attach the file. Could you review the file or send the load file of the TICS Pro?

Best Regards

Jae-Heung YeomLMX2615_65_472M.tcs