This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: Mount the LMX2592 on the LMX2572 circuit board

Part Number: LMX2592
Other Parts Discussed in Thread: LMX2572,

Tool/software:

Dear Team,

My customer has evaluated the LMX2572 and has the prototype board of the LMX2572.
This time, they want to evaluate the LMX2592 and want to mount the LMX2592 on the LMX2572 circuit board.
There are the following pin differences between the two products.

      <LMX2592>  :  <LMX2572>
Pin 32: NC          :    RampDir
Pin 30: NC          :    RampClk
Pin 28: NC          :    SysRefReq
Pin 5  : NC          :    SYNC 

Is it possible to perform evaluation even if the LMX2592 is mounted on the LMX2572 circuit board?

Best Regards,

Koshi Ninomiya