LMK5B33414EVM: 1PPS jitter cleaner with Zero Delay Mode typical configuration example

Part Number: LMK5B33414EVM
Other Parts Discussed in Thread: LMK5B33414

Hello,

I have a LMK5B33414EVM evaluation board, and I'd like to do a quite simple test but I can't find a configuration that works on TICS Pro. Here is what I want to do:

 

I have a 1 PPS signal coming from a uBlox GNSS receiver (ZED-F9P), with a +/- 10ns jitter approximately. I want to use the LMK5B33414EVM to clean the jitter of this 1PPS signal (thanks to the DPLL with low bandwidth of 0.01Hz for example), and to obtain on an output of the LMK5B33414 a jitter-cleaned 1PPS signal aligned in phase with the 1PPS input signal.

I assume that I need to use a combination DPLL + APLL to clean the jitter, thanks to the low bandwidth of the DPLL, of 0.01 Hz for example. And in order to guarantee the phase alignment of the ouput 1 PPS signal with the input one I assume that the Zero Delay Mode (ZDM) should be used too. But I can't find a configuration that works well with TICS Pro, although I'm sure it's a quite standard request for this kind of component.

The 1PPS output signal can be set on any output of the LMK5B33414, it doesn't matter. And I can use any frequency for the XO (either the on-board 48MHz OCXO or any external XO frequency can be used), so I'm open to any configuration that could perform this jitter-clean function + alignment of the 1PPS signal.

Can you give me an example configuration file of TICS Pro that works this way ?
Thanks a lot for you help !

 

Best regards,

Antoine