Part Number: SA555
Other Parts Discussed in Thread: TLC3555-Q1, TLC555
Hi team,
I have 3 questions.
I want to drive Astable Operation with 20us:L, 40us:H. Planning to use RA, RB:1330orm, C:0.022uF.
- In addition to the R and C tolerances, what parameters are taken into account to calculate the output variation?
- What are the recommended resistance and capacitance values? Of the system. What are the advantages and disadvantages of using higher resistance or capacitance?
- Is there information on the actual resistance range between pin1-2, 2-6, 6-8 ? I understand that they all have the same resistance value.
Regards,
Hiromu