This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04808: LMK04808 : Design Queries

Part Number: LMK04808

Hi Team,

  1. What will be the output at OSCOUT0/OSCOUT0# if I will be providing 20MHz clock to OSCIN/OSCIN# and single ended 100MHz clock to CLKIN0?
  2. Is there any hardware strap option or software register setting to select the clock reference for OSCOUT0?
  3. If both 20MHz and 100MHz input clocks are present, does it have any auto mode where it selects the reference clock based on internal priority

Thanks