Part Number: LMX2615-SP
Other Parts Discussed in Thread: LMK04832
Hi Experts,
I'm using a single LMX2615 in a design, and had a question regarding VCO_PHASE_SYNC. In my application, the part takes in a 100 MHz reference, uses the x2 input frequency doubler with no PreR or R divider, and generates a VCO output of 10 GHz using an N divider of 50. Output A is set to output this VCO clock directly (10 GHz, no channel divider), but Output B is set to output 5 GHz (/2 in the channel divider). In this case, is utilization of VCO_PHASE_SYNC required? Per page 27 of the datasheet, it seems implied that this would be considered Category 1 with Sync mode required, but is this correct?
Lastly, just to mention again, I'm only using a single LMX2615 device. However, I do require deterministic latency in this application if that affects the answer. For that, the output of the LMX2615 in the design provides a clock input to an LMK04832, which then distributes the SYSREF and device clocks.
Attached is the output of the register settings I'm using for quick reference.
LMX2615 HexRegisterValues SPI Readout CS20251211.txt
Regards,
Carl