Part Number: LMX2592
Hi Team,
looking at the max abs values from the LMX2592 DS:
We can see that the max voltage on OCin is 1.8Vpp, however in the example under 7.3.1:
The voltage swing is 2Vpp, am i reading this correctly?
What will be the typical requierd Vpp for OSCin?
also, i can see that when VCC = 0V then the OSCin should be less than 1Vpp, what is the meaning here? cant i input a clock signal without VCC on the LMX device?
Thanks!