Part Number: LMX2592
During my testing, I found that the voltage at the VbiasVCO pin of LMX2592 was 0.26V, while the voltage at VbiasVCO2 was 0.7V. I'm not sure if this is correct, and I'm also curious if this will cause the phase-locked loop to lose lock or lead to other abnormal phenomena. Therefore, I would like to ask what the voltage should be for these two pins when the phase-locked loop is in a normal locked state.