Part Number: LMX2592
Other Parts Discussed in Thread: , LMX2595, LMX2594, LMX2572
Ryusuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2592
Other Parts Discussed in Thread: , LMX2595, LMX2594, LMX2572
Hi There,
OSC input
What is your clock format and amplitude?
RF output
There is no performance difference between RFoutA and RFoutB, you can use either one.
The unused output can be programmed to power down, the pins can be left floating.
If only one of the output pins is used, the unused pin still need pull-up and termination. P and M pin has not performance difference except they are out of phase.

Pin 30
there is no physical connection inside the chip, you can leave this pin floating, short to ground directly or via a resistor.
Hi Noel,
Thank you for your reply.
They using a 10 MHz OCXO as a reference, PLL (ADF4111) +VCO generates 300 MHz.
1: 353.7 MHz (fixed)
2: 340.0 MHz (fixed)
5: 1262.5 MHz (fixed)
are distributed and amplified and fed by Sine waves.
DDS generates a 30 MHz band signal for the above signal.
3: 1795~1995 MHz or 1845~1945 MHz
4: 1820~2020 MHz or 1870~1970 MHz
and is supplied by Sine wave.
Amplitude
→I don't know how to answer.
DC cut capacitor is inserted at the output of the supply source and the input of the LMX2592.
Best Regards,
Ryusuke