This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: Vibration noise avoidance on LMK04832

Part Number: LMK04832

Hello:  The datasheet specifies a 10uF cap on LDObyp1.   But, if this is a reference for the internal LDO, any noise on this pin will be forced onto the LDO output by the feedback of the LDO, which basically functions as just a power buffer on this node.  So, if a high dielectric (microphonic/piezo electric) ceramic like X7R is used here, then vibration induces electric noise here which can be many tens of dB's over the noise floor.  So, my question is whether this "bypass" is on the output (where a vibration sensitive capacitor is OK as then the loop suppresses vibration noise), or the reference (where then the loop copies the noise to the output).  If it a reference node, then a film capacitor should be used here to avoid vibration noise.