Part Number: LMK04832
Other Parts Discussed in Thread: LMK04828, ,
Hello: We have used the LMK04828 with an HSDS-8mA output before with the below type interface for 250MHz clocks. It has a resistor across the two pins of an output port, then AC coupling caps from each pin to the target. However, the LMK04832 we are changing to reports on datasheet pages 14-15 that the LMK04832 in HSDS 8mA output mode is specified with DC bias on the output pins, specifically 50 ohms to a (Vcc-1.64) voltage level (nominally 1.66V). In transistor current source outputs they are generally valid into a range of voltage, sometimes called the "Compliance Range". There is no such spec in the LMK04832 datasheet--just the note that the datasheet swings are with the 1.66V exteranal bias applied. It is fine to not bias the pins in LVDS mode, as in that mode they are internally biased to 1.25V nominal. But the datasheet is apparently expecting 1.66V DC bias for HSDS-8mA. Despite this, no DC bias is also used in the LMK04832EVM User's Guide for HSDS ports (such as channels 8 and 9). So, it is best design practice to ignore that DC bias callout in the datasheet, such as is done in EVM User Guide schematics? Or, should we plan to bring in bias for HSDS pins? Is there a performance penalty for not using the datasheet bias? Thanks, Farron.