Customer request;
I have two (or three) power supplies that I would like to sync to an external clock. This way the power supplies can be run 180 degrees (or 90 degrees) out of phase from each other to reduce ripple current in the power system.
Is there a synchronizer chip that puts out two (or three) clocks that are 180 degree (or 90 degrees) out of phase with each other to take care of this?
The switcher runs at 300KHz but the SYNC pin will take 200KHz – 400KHz. The input logic levels on the SYNC pin are TTL. Commercial temperatures should be okay here.
Comments.....
-Tom-