Hi Team!
I had a few questions regarding the LMK03002.
On the datasheet, it states that bit 31 is the RESET bit in register R0. Is this the only thing that is present in register 0?
Also, on page 15, section 2.3. It states that "Registers R4 through R7 control the four clock outputs. Register R3 controls CLKout0, Register R4 controls CLKout1, and so on." Is this a mistake? Should the correct statement say the following "Registers R4 through R7 control the four clock outputs. Register R4 controls CLKout0, Register R5 controls CLKout1..." ?
Thank you for all your support!
Ben