I am having issues with getting ClockPro to run properly with my CDCE EVM board.
My EVM board is one of the first releases I think back in 2009.
At that time I loaded the first version of the sw but that was removed and so I had to update to the latest.
I just downloaded the SW and Drivers to my XP machine, unzipped the drivers in a folder.
I used Windows wizzard to find the unpacked drivers however it won't load them from this folder.
Instead the Win Wizzard finds one in the windows driver directory, perhaps the original driver or something inappropriate, I think this is the problem.
Q - Why can't it pull the new driver out my folder? Is there some ID problem on the EVM?
I checked the Device Manager and see that the EVM calls it self TI CDCE(L)9xx Family_EVM-Serial Port.
Using the driver found in Win system, I ran the SW install and noted the installation of .Net framework 4 and TUSB3410.
I found another string on this topic http://e2e.ti.com/support/clocks/f/48/t/183453.aspx and his EVM is calling out TUSB3410.
Q - Do I need to get the latest board?
When I run the SW and try to have it find the board I get an Exception warning and the SW crashes
Top line says: Index was outside the bounds of the array. at CDCE949Project.ProgramminEVMDevice.GetFirmware Veersion (Boolean& is1p1) Etc - see below
This happens with the EVM board connected or not. Whe the EVM connected to USB and initialiation of the SW, the Green circle stays dark.
I assume I have the wrong driver but don't know how to resolve this