Hi,
I have a question regarding the LMK03002. We are using it on a new design to produce a 200MHz clock from a 10MHz input reference. I believe I have the registers set up correctly to do this:
CMD_REG_R0 = x"8000_0000";
CMD_REG_R4 = x"0003_0204";
CMD_REG_R8 = x"1000_0908";
CMD_REG_R11 = x"0082_000B";
CMD_REG_R13 = x"0282_800D";
CMD_REG_R14 = x"0830_010E";
CMD_REG_R15 = x"C800_500F";
We are getting a clock output but it is 226.76MHz. What could be causing this discrepancy?
Thanks,
Jody