This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208 pin mode

Other Parts Discussed in Thread: CDCM6208V1

Hello.

 

I have used CDCM6208V1 & V2 clock buffer in my design.

These chip setting was pin mode.

But output is not setting the value.

 

V1:

-PRI_REFP/N : 25MHz LVDS

-SEC_REFP/N : NC

-PIN[4:0] : 0x09(10-V1) -> Y0/1: 125 LVDS,  Y2/3: 156.25 LVDS, Y4/5: 100 LVDS  Y6: 133.33 LVDS Y7: 25 LVDS

-PDN/SYNCn : 4.7k pull up(3.3V)

-SI_MODE[1:0] = 10 (pin mode)

-REF_SEL : 4.7k pull down

-RESETn/PWR : 3.3V

-ELF : 100p/500/22n

-power : all 3.3V

 

But STATUS0 is LOW. And output Y0 and Y1 is 130MHz. Also Y2 to Y7 is 104MHz.

Please let us know if there is any issues.

 

Thanks.