1. I have purchased a cdcel9xxprogevm (CDCE(L)949 Family EEPROM Programming Board) and I have not been able to use it because there is some driver problem.
The manual said I should install the driver from the CD that came with the board, but I did not see a CD in the box.
Please send me a link for a driver I can use.
2. I have a 64 bit windows 7, and I tried both TI Clock Pro software 1.0, and the latest TI Clock Pro (on my co-worker's window 7 computer). I know the 1.8V and 3.3V supply on the board is good because the two LEDs on the board turned on. I tried plugging in hardware after starting TI Clock Pro software, and vice versa.
3. I have tried using these three drivers from http://www.ti.com/product/TUSB3410/toolssoftware and they did not work.
4. Here are some screenshots of my TI Pro and my Device manager: