Hi,
I am using LMK04000BISQE IC in my design. I has 5 clock output among these 5 channels, I am using only second and third clock output port in a single ended CMOS input type.
Remaining three clock output ports are not going to be used. So, through register settings, I can disable the output port. In addition to that any other termination schemes to be done for the unused clock output ports.
If Yes, then give me the suggested method to terminate the unused LVPECL output and unused single ended CMOS clock output.