Hi,
I am trying to use LMK04808 board to configure output clock frequency
Dual loop mode ,0-delay, int vco
PLL1 input frequency 936 MHz, PLL1 vco 936 MHz
PLL2 input frequency 80 MHz VCXO, VCO 2808 MHz
when I load the registers, everything looks good. Output is set to 936 MHz and output tracks with input . Great!
if I disconnect the uWire programming cable, PLL gets into Holdover mode and the output frequency goes to ~1880 MHz. I am not sure why this happens
I am trying to program LMK04808 with the same register set with an FPGA and the result is the same(directly goes into holdover mode once all the registers are loaded from fpga). I am struggling to understand why the clock conditioner is behaving this way. it would be great, if someone can please look into this.
Thanks,
Ramakrishna