Hi,
I can see in the data sheet for the CDCLVD2102 that its "specifically designed for driving • One Input Dedicated for Two Outputs 50-Ω transmission lines. If driving the inputs in single • Total of 4 LVDS Outputs, ANSI EIA/TIA-644A ended mode, the appropriate bias voltage (VAC_REF) Standard Compatible should be applied to the unused negative input pin." But I'm not seeing an indication of how many lines. In the LVPECL to LVDS example (figure 18) it shows 2 50-Ω lines, can it handle 4?
Thanks,