Hi,
This is the first time I'm using CDCM61004. I need 50MHz LVPECL output frequency. I would like to use 20MHz or 12MHz crystal as input
With Crystal is 25MHz, I see that CDCM61004 can not generate 50MHz
With Crystal is 12MHz, PR[1:0] = 10, OD[2:0] = 101, CDCM61004 ouput is 50 MHz
Could you please help me review above crystal frequency input, output divider, and feedback divider configuration?
Regards,
Ty