This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock jitter cleaner products

Other Parts Discussed in Thread: LMK04906, LMK04002, LMK03200

Hi,

I would like to ask you to give me your adivce about "jitter cleaner".

My customer has a problem with jitter of clock signal.

Could you recommend jitter cleaner device to meet following speifications?

 - Input frequency : 100MHz - 200MHz, over 1ch

 - Output frequency : 50MHz - 100MHz, over 1ch

 - The jitter performance of output is to meet the specification of "FPGA(AIRTIX7) GTP clock".

 - Signal level : Any is OK.

 - The input signal changes linearly and the output signal has to follow the change.

I suppose the following devices are candidate.

That is to say, LMK03200, LMK04002, LMK04906.

Would you give me your idea about the devices and I am very glad if you tell me your recommend devices.

Thank you for your support.

Best Regards,