Other Parts Discussed in Thread: LMK04906, LMK04002, LMK03200
Hi,
I would like to ask you to give me your adivce about "jitter cleaner".
My customer has a problem with jitter of clock signal.
Could you recommend jitter cleaner device to meet following speifications?
- Input frequency : 100MHz - 200MHz, over 1ch
- Output frequency : 50MHz - 100MHz, over 1ch
- The jitter performance of output is to meet the specification of "FPGA(AIRTIX7) GTP clock".
- Signal level : Any is OK.
- The input signal changes linearly and the output signal has to follow the change.
I suppose the following devices are candidate.
That is to say, LMK03200, LMK04002, LMK04906.
Would you give me your idea about the devices and I am very glad if you tell me your recommend devices.
Thank you for your support.
Best Regards,