This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV112 Dual Clock Buffer

Other Parts Discussed in Thread: LMV112, CDC3RL02, CDCLVC1102, LMK00804B, LMK00105

Hello,

Can LMV112 Clock Buffer be used with CMOS Oscillator (like DSC1003)?

Thank you,

GMC

  • This is an analog unity-gain buffer, which could work if you don't need level translation and operating with lower frequency clocks (~30 MHz).

    If you need a buffer that supports higher frequency and LVCMOS logic levels, you can consider:
    CDC3RL02 - 1:2 fanout, 1.8V LVCMOS
    CDCLVC1102 - 1:2 fanout, 2.5/3.3V LVCMOS
    LMK00804B - 1:4 fanout, 1.5/1.8/2.5/3.3V LVCMOS
    LMK00105 - 1:5 fanout, 1.5/1.8/2.5/3.3V LVCMOS

    Alan