Hello,
in the datasheet of the CDCM61004 the max. junction temperature is NOT specified. What is the max. allowed junction temperature?
In my application the case temperature (top) is 90°C (worst case). The power loss of the chip is max. 0,66W (3,3V *0,2A).
By using the Junction-to-case (top) thermal resistance I can calculate the junction temperature.
Tjunction = 90°C+0,66W*25,7°C/W = 107°C
The question is if 107°C junction temperature is allowed or not?
Thanks!
Greetings from Austria,
Daniel