This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS64EV400: DS64EV400, DS64EV100 min Data rate

Part Number: DS64EV400

Hi,

Let me check the corresponding bit rate of each device.
Are the following 4 products available at 2 Gbps or 1.5 Gbps?

DS32EV100
DS25BR400
DS64EV100
DS64EV400

The user's required specifications are CML input / output (sufficient for the buffer function), at a rate of 1.5 Gbps,
ESD (HBM) is over 5 kV.

In addition to the above four products, please tell me the device you recommend.

Best regards