Other Parts Discussed in Thread: TL431-Q1, OPA2377-Q1, NE555, TLC555
Hi,
Customer would like to use TLC555-Q1 for oscillator about 100Hz~200Hz.
It has to used in full thermal range so tolerance is important.
In the datasheet, threshold voltage is from 2.7V ~ 3.9V at Vdd=5V.
How many does this voltage range make the tolerance if there is not a tolerance of external component?
In my calculation, R1=2.89k, R2=11.54k, C=1uF, frequency is 100Hz.
I adopted 2.7V~3.9V to Vc and frequency is varied from 91Hz~107Hz in a result. +/-10%
Am I correct?
For reducing tolerance, I will recommend to add TL431-Q1 for 3.3V reference and OPA2377-Q1 for filter to CONT pin.
If these are adopted, can I assume that tolerance is 0.5% without tolerance of external component?
Thanks.