Other Parts Discussed in Thread: LMK03328
Please advise me on a question bellow:
I want to generate 148.5 MHz and 148.35174 MHz from 27 MHz reference
using CDCI6214 enabling fractional divider in it.
I have chosen the 2700 MHz VOC frequency. So the input frequency
is one eighth (337.5MHz)
So, 145.5 MHz and 148.35174 MHz can be obtained by divided by
44/1000 and 440/1001 respectively.
However, I do not know how to specify numerator and denominator
In the Clock Pro GUI.
The GUI suggested the numerator and denominator itself.
However, there is small frequency error.
I need to specify the precise numerator and denominator.
Mita