Other Parts Discussed in Thread: LMK00306
I'm using the LMK62A2-200M in a product design to drive the LMK00306. The LMK00306 says the clock inputs require a driving clock signal with a 3V/ns slew rate (section 9.1). In the datasheet for the LMK62A2-200M section 6.8 it says HCSL outputs have a slew rate from 1V/ns to 3V/ns, but it says nothing about LVDS. I need to drive an LVDS clock from LMK62A2-200M to the LMK00306. How do I know if the LVDS output from the LMK62A2-200M won't cause excessive phase noise?
Thanks!