I was able to get stable clock output with 800MHz input, but shaking clock output or nothing with 640MHz input. LMK is powered up at 3.3V with current measured at 4400mA (power down=0.96mA). Below is lmk programming.
void LMK::lmkspi_TICS_Pro()
{
SPI::wspi_lmk(0x0000, 0x90);
SPI::wspi_lmk(0x0000, 0x00);
SPI::wspi_lmk(0x0002, 0x00);
SPI::wspi_lmk(0x0003, 0x06);
SPI::wspi_lmk(0x0004, 0xD0);
SPI::wspi_lmk(0x0005, 0x5B);
SPI::wspi_lmk(0x0006, 0x00);
SPI::wspi_lmk(0x000C, 0x51);
SPI::wspi_lmk(0x000D, 0x04);
SPI::wspi_lmk(0x0100, 0x64);//DCLKOUT0 divider=4
SPI::wspi_lmk(0x0101, 0x44);
SPI::wspi_lmk(0x0102, 0x55);
SPI::wspi_lmk(0x0103, 0x00);//02);
SPI::wspi_lmk(0x0104, 0x20);//22);
SPI::wspi_lmk(0x0105, 0x00);
SPI::wspi_lmk(0x0106, 0xF0);
SPI::wspi_lmk(0x0107, 0x11);
SPI::wspi_lmk(0x0108, 0x01);//0C);
SPI::wspi_lmk(0x0109, 0x55);
SPI::wspi_lmk(0x010A, 0x55);
SPI::wspi_lmk(0x010B, 0x00);
SPI::wspi_lmk(0x010C, 0x20);//22);
SPI::wspi_lmk(0x010D, 0x00);
SPI::wspi_lmk(0x010E, 0xF0);
SPI::wspi_lmk(0x010F, 0x60);
SPI::wspi_lmk(0x0110, 0x64);//DCLKOUT4 divider=4
SPI::wspi_lmk(0x0111, 0x44);
SPI::wspi_lmk(0x0112, 0x55);
SPI::wspi_lmk(0x0113, 0x00);//01);
SPI::wspi_lmk(0x0114, 0x00);//02);
SPI::wspi_lmk(0x0115, 0x00);
SPI::wspi_lmk(0x0116, 0xF1);
SPI::wspi_lmk(0x0117, 0x16);//CWEI: DCLKOUT4=LVPECL20=0x16; LVDS=0x11
SPI::wspi_lmk(0x0118, 0x64);//DCLKOUT6 divider=4
SPI::wspi_lmk(0x0119, 0x55);
SPI::wspi_lmk(0x011A, 0x55);
SPI::wspi_lmk(0x011B, 0x00);
SPI::wspi_lmk(0x011C, 0x00);//02);
SPI::wspi_lmk(0x011D, 0x00);
SPI::wspi_lmk(0x011E, 0xF1);
SPI::wspi_lmk(0x011F, 0x06);//CWEI: DCLKOUT6=LVPECL20=0x06; LVDS=0x01
SPI::wspi_lmk(0x0120, 0x08);
SPI::wspi_lmk(0x0121, 0x55);
SPI::wspi_lmk(0x0122, 0x55);
SPI::wspi_lmk(0x0123, 0x00);
SPI::wspi_lmk(0x0124, 0x20);//22);
SPI::wspi_lmk(0x0125, 0x00);
SPI::wspi_lmk(0x0126, 0xF0);//F8);
SPI::wspi_lmk(0x0127, 0x60);
SPI::wspi_lmk(0x0128, 0x08);
SPI::wspi_lmk(0x0129, 0x55);
SPI::wspi_lmk(0x012A, 0x55);
SPI::wspi_lmk(0x012B, 0x00);
SPI::wspi_lmk(0x012C, 0x00);//02);
SPI::wspi_lmk(0x012D, 0x00);
SPI::wspi_lmk(0x012E, 0xF9);
SPI::wspi_lmk(0x012F, 0x00);
SPI::wspi_lmk(0x0130, 0x64);//DCLKOUT12 divider=4
SPI::wspi_lmk(0x0131, 0x55);
SPI::wspi_lmk(0x0132, 0x55);
SPI::wspi_lmk(0x0133, 0x00);
SPI::wspi_lmk(0x0134, 0x20);//22);
SPI::wspi_lmk(0x0135, 0x00);
SPI::wspi_lmk(0x0136, 0xF0);
SPI::wspi_lmk(0x0137, 0x11);
SPI::wspi_lmk(0x0138, 0x40);
SPI::wspi_lmk(0x0139, 0x03);
SPI::wspi_lmk(0x013A, 0x00);//SYSREF div by 480=0x13A(0x01)+0x13B(0xE0)
SPI::wspi_lmk(0x013B, 0xA0);//SYSREF div by 160=0x13A(0x00)+0x13B(0xA0)
SPI::wspi_lmk(0x013C, 0x00);
SPI::wspi_lmk(0x013D, 0x08);
SPI::wspi_lmk(0x013E, 0x03);
SPI::wspi_lmk(0x013F, 0x07);
SPI::wspi_lmk(0x0140, 0xF3);//F1);
SPI::wspi_lmk(0x0141, 0x00);
SPI::wspi_lmk(0x0142, 0x00);
SPI::wspi_lmk(0x0143, 0x10);
SPI::wspi_lmk(0x0144, 0xFF); //7F);
SPI::wspi_lmk(0x0145, 0x7F);
SPI::wspi_lmk(0x0146, 0x00);
SPI::wspi_lmk(0x0147, 0x13);
SPI::wspi_lmk(0x0148, 0x02);
SPI::wspi_lmk(0x0149, 0x42);
SPI::wspi_lmk(0x014A, 0x02);
SPI::wspi_lmk(0x014B, 0x02);
SPI::wspi_lmk(0x014C, 0x00);
SPI::wspi_lmk(0x014D, 0x00);
SPI::wspi_lmk(0x014E, 0xC0);
SPI::wspi_lmk(0x014F, 0x7F);
SPI::wspi_lmk(0x0150, 0x00);
SPI::wspi_lmk(0x0151, 0x02);
SPI::wspi_lmk(0x0152, 0x00);
SPI::wspi_lmk(0x0153, 0x00);
SPI::wspi_lmk(0x0154, 0x78);
SPI::wspi_lmk(0x0155, 0x00);
SPI::wspi_lmk(0x0156, 0x78);
SPI::wspi_lmk(0x0157, 0x00);
SPI::wspi_lmk(0x0158, 0x96);
SPI::wspi_lmk(0x0159, 0x00);
SPI::wspi_lmk(0x015A, 0x01);
SPI::wspi_lmk(0x015B, 0xD4);
SPI::wspi_lmk(0x015C, 0x20);
SPI::wspi_lmk(0x015D, 0x00);
SPI::wspi_lmk(0x015E, 0x00);
SPI::wspi_lmk(0x015F, 0x0B);
SPI::wspi_lmk(0x0160, 0x00);
SPI::wspi_lmk(0x0161, 0x01);
SPI::wspi_lmk(0x0162, 0x44);
SPI::wspi_lmk(0x0163, 0x00);
SPI::wspi_lmk(0x0164, 0x00);
SPI::wspi_lmk(0x0165, 0x0C);
SPI::wspi_lmk(0x0171, 0xAA);
SPI::wspi_lmk(0x0172, 0x02);
SPI::wspi_lmk(0x017C, 0x15);
SPI::wspi_lmk(0x017D, 0x33);
SPI::wspi_lmk(0x0166, 0x00);
SPI::wspi_lmk(0x0167, 0x00);
SPI::wspi_lmk(0x0168, 0x04);
SPI::wspi_lmk(0x0169, 0x59);
SPI::wspi_lmk(0x016A, 0x20);
SPI::wspi_lmk(0x016B, 0x00);
SPI::wspi_lmk(0x016C, 0x00);
SPI::wspi_lmk(0x016D, 0x00);
SPI::wspi_lmk(0x016E, 0x13);
SPI::wspi_lmk(0x0173, 0x60);
SPI::wspi_lmk(0x1FFD, 0x00);
SPI::wspi_lmk(0x1FFE, 0x00);
SPI::wspi_lmk(0x1FFF, 0x53);
}