Other Parts Discussed in Thread: LMX2592
Hello
I would like to use LMX2594 with 100MHz reference in LVPECL. The distance between the LVPECL driver to the OSC pin of LMX2594 can be 4-5 inch stripline.
So I thought about placing two 150ohm resistors to ground near the transmitter, two dc blocks and then route stripline 100ohm differential line to the LMX2594.
Now I am confused about the input circuit of the OSC pins of LMX2594. No information on the datasheet (there is some info on the datasheet of LMX2592) - on the EVB there are 50 ohm to ground or 100ohm between the two OSC pins. What is the correct way? please review the entire path from the transmitter all the way to the LMX2594.
Thanks