This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVD2104: EN control input voltage level

Part Number: CDCLVD2104


Hi,

Could you tell me about the voltage that detects "Open"?
The typ of VdI3 is 0.5 × Vcc, but I want to know min and max.
Is there information for these values?
It does not have to be a guaranteed value.



Best regards,
Yuto Sakai

  • Hi Yuto,

    I'm afraid there is no such information. Pin "EN" has internal pull-up and pull-down resistors, so if you want to use Tri-state, just leave the pin open. I don't see where the min and max values are needed.

    Regards,
    Hao