This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK62A2-200M: Enable Pull-up / Datasheet typo

Genius 16285 points
Part Number: LMK62A2-200M

Hi all

Referring to below feedback from a customer it seems the Datasheet is somewhat misleading:

OE 1 LVCMOS Output enable (internal pullup). When set to low, output pair is disabled and set at high impedance.

Should this read: OE should be connected to VCC to enable the device ?

Please clarify.

Best regards

Ueli

-------------------------------------

We fitted the oscillator LMK62A2-200M in a new board we built. We left OE pin 1 not connected because the datasheet says that there is an internal pullup. However with pin 1 floating there is no output. When we pull OE to 3.3V the oscillator output is active. Is this a known issue? Is there a mistake on the datasheet or there is something else wrong with our board?