Other Parts Discussed in Thread: USB2ANY, LMK04208, LMK04816, CODELOADER, USB2ANY-UWIRE
I cannot program my LMK04816B Eval board. I am trying to do the quick start scenario in the manual using a USB2ANY adapter.
I have replicated the quick start scenario where I have a 122.88 MHz clock signal being input on CLKIn1.
I am monitoring CLKout6 to see what the resulting output frequency is. All I see out of it is a 122.88 MHz signal no matter what I attempt to program into it..
I have tried both CodeLoader4 and TICs Pro.
When I start up TICs Pro, I encounter the following error:
Conflicts exist between the following pins:
Pin J4-8: GPIO(GPIO5) conflicts with SPI(SOMI)
I never see the Link Detect LED light.
I can do the same exercise with a LMK04208 eval board and it works as expected. (Same power supply, same reference input, same output monitor.)
Any suggestions for things I can try?