Hi Sir/madam,
We are using this clock buffer for 25MHz clock and using 3 outputs for 3 different devices. Clock input is from 3.3V crystal oscillator.
Clarifications:
1. Can i give 3V (typical) as Vcc for this device? There may be Vcc voltage variation 2.8V (min) ~3.2V (max). Can this device work properly as expected in this case? Please confirm.
2. If i give supply as 3.3V, then out of 3 clocks, 2 devices will work in 3.3V domain (Also can work in 3V) but one device requires 3V domain only and maximum it will accept 3.15V. But this buffer output may reach 3.6V which will damage the receiver. Do you have any suggestion to solve this issue?
Thanks & Regards,
Remya