Hi
I bought TRF3765EVM REV E.
I think +5.0V Connection to Regulators is not connected. I tested the connection is open.
Is there any other problem if I connect 5V of USB output to + 5.0v?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I bought TRF3765EVM REV E.
I think +5.0V Connection to Regulators is not connected. I tested the connection is open.
Is there any other problem if I connect 5V of USB output to + 5.0v?
Hi BH,
To use these regulated 3.3-V supplies, disconnect power from TP2 and remove R41. Connect 5 V to TP26, using TP27 for ground. Place jumpers on JP4 and JP5 to shunt jumper pins 1 and 2.
If you use the 5V from a USB device, make sure it is capable of supplying 250 mA.