This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208V1EVM: How should the pins of VDD_PLL and VDD_VCO be connected?

Part Number: CDCM6208V1EVM

Dear engineer !

  Recently I am looking at the CDCM6208EVM file. I have two questions about the schematic diagram of the file

1.as shown in the figure, Is this pin connected as shown in the picture and then the external power supply is connected to the VDD_PLL pin and so is VDD_OUTA/B?

2.In order to save PCB board space, can I use only one power chip(TPS7A8001) to output 1.8v to VDD_SEC, VDD_VCO, VDD_PLL1 and VDD_OUTA at the same time?

Thanks