Hello;
CDCE925 Flexible Low Power LVCMOS Clock Generator I want to make 100Mhz wave generator using EMI Reduction with SSC Support. I need to produce square wave, triangle wave and sine signals. Can I increase the frequency of the signal if I input the signal outputs of the AD5932 to the VCO input of the CDCE925? So does the CDCE925 IC accept all three types of signals as inputs?
Sincelery