This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High-Speed PCB Routing Guidelines



Hi

I'm doing an HDMI board design and I've encountered what I think is a very large intra-pair skew requirement. The HDMI spec states 0.15Tbit which at 6GHz is 25ps. As a rule of thumb this would equate to about 3.8mm of FR4 (150um/ps). In TI's doc http://www.ti.com/lit/an/slla414/slla414.pdf section 2.4 (displayport) suggests 5mil (125um) for 20ps. I do not know why 125um is suggested for a 20ps skew when it only needs to be 3mm!

Have I made a glaringly obvious mistake?