Hi Team,
Just a clarification on the recommended supply voltage for TPL5000. Section 7.3 of the datasheet rated the supply range at 1.8V to 5V, while section 10 says it should be within 2.7V to 5.5V. Can you confirm which is the appropriate recommended range? Our customer intends it to use on a project running in 2.2V supply so this would be a determining factor on whether the device can be used or not.
Thank you very much for your help.
Kind Regards,
Jejomar