Other Parts Discussed in Thread: LMK04828
Hello,
In LMX2581 Datasheet, there are below data relevant to OSCin pin:
- a graph showing the input impedance vs. freq. (mag = 300 - 600 ohm for freq. less than 100 MHz),
- min. & max. amplitude (0.4 - 1.8 V) of ac-coupled clock, and
- the acceptable freq. range of clock.
Moreover, two notes are seen as following:
- higher slew rate leads to better noise performance, and
- recommendation of external components to make the OSCin impedance 50-ohm.
However, I am not able to choose the proper TCXO as the clock maker. Let me ask:
- Which output kind of TCXO should I consider, e.g. CMOS, 10kOhm || 10pF, ECL, LVDS ...?
- Why the aforementioned 50-ohm impedance is recommended?
- Suppose I select a TCXO with Vs = 1.8V, OL = 10kOhm || 10pF, Waveform = Square and ac-coupled it via a series resistance of 200-800 Ohm to OSCin. What would be the problems, if any?
Thanks in advance to anybody who reply to me.