Part Number: CDCI6214EVM
Hello,
I try to make the CDCI6214EVM work by following the steps indicated in the datasheet.
Here is what I did :
* I selected 1V8 by moving J26 shunt on "+" (I guess it is needed to have supply)
* I leave the J16 SYNC shunt on VDD.
* Selected CDCI6214EVM in TICSPRO
* I connect the device with USB : recognized OK
* I charge a default config
* I put the DUT ON : I2C tested OK
* I write the config into the EVM : write OK
Then I try and measure the outputs :
*Nothing on SMA Xin or Xout
* SMA_Y1N is constant 1V8 (instead of LVDS 156MHz)
I don't understand. Even with the default config, I don't manage to get an output.
Is there something I am missing ? Did I do something wrong with shunts ?
Some help would be great. Thank you.
Arthur