Hi all!
On my device I need to use two CDCE706; on both of them I need the CLK_SEL input as I have two different clock and I must allow the user to choose the one he wants to use.
I see that the S1/A1 input can be used as a SMBus device address, so I think I could connect both CDCE706 to the same bus and use that pin as a "device select".
But it is not clear to me whether the CLK_SEL function on S0 and address function on S1 can be used together at the same time. Can you please clarify?
Thanks in advance.
Best regards,
Stefano Infante