This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2491: I can't see anything from the multiplexer output

Part Number: LMX2491

Hello, tell me, please, I made my board with LMX2491 and BGT24MTR12, but I can't run the PLL. I program the registers in reverse order r141-R0, everything is passed correctly (checked with a logic analyzer, the picture shows an example of transmission). Configured the pin MOD for the input (I submit hours of 40 kHz) and to check the output of the multiplexer configured as an output from the pin mod, but I do not see anything, although it should be clock of 40 kHz. On PLL comes 3.3 V, ostin 100 MHz, current consumption is growing(concluded that LMX2491 understands me). Circuit design as in the documentation.