Other Parts Discussed in Thread: CDCM6208, LMK02000, ADS127L01, PLL1707, CDCE925, CDCE6214-Q1, SN74LVC374A-Q1
Hi,
I am looking for a relatively simple but good quality clock generator solution capable of supplying all clocks for ADC/DAC via I2S:
* master clock 36.864MHz
* I2S bit clock 48 x FS, i.e. from 48 x 48kHz to 48 x 768kHz = 2.304MHz to 36.864MHz
* I2S LR clock 1xFS, i.e. from 48kHz to 768kHz
IIUC the FS clock is too slow for ultra-low jitter VCO generators (LMK03806, CDCM6208) which have the output divider up to some 1041 which does not allow going below some 1.5MHz from the GHz VCO.
Neither the two-PLL generators LMK02000,...) do not go so low (at least the Clock Design Tool does not offer any solution).
Please what solution would be the most recommended? I can imagine an external divider for the LR clock (/32, /64) - please what chip would be best for doing the division while maintaining low jitter?
Or just a chip for clock division of 36.864MHz crystal signal, no PLL would be required. I could not find any any clock-related chip on TI.com offering such large divider ratio for one of the outputs.
Thank you for any help.
With regards,
Pavel.