Other Parts Discussed in Thread: CDCE62002
Hi,
I am trying CDCE62002EVM and I am having the following issues:
1. The registers value after cycling the power from software is as attached.
I am loading the default settings and writing them to eeprom and yet still the same old values getting loaded on power up.
2. No matter which settings I use, the on board locked is always off even if the status on gui hows on.
I am powering the board from usb and using the on board crystal as reference, the clock outputs are floating.
the frequencies I want to generate are 100 MHz and 25 MHz both lvcoms.
Thanks,